FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Screen gesture function when the video/RGB input screen is displayed
FAQ
Screen gesture function when the video/RGB input screen is displayed
Can the video/RGB input screen size be enlarged or reduced by using the screen gesture function?
Answer
The screen size cannot be enlarged or reduced because the video/RGB input screen (including multimedia) is hidden during the screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (video/RGB)
- Series
- GOT2000 Series