FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Enabling and disabling the single touch operation for the cursor display
FAQ
Enabling and disabling the single touch operation for the cursor display
Can I enable or disable the single touch operation for the cursor display with a device value?
Answer
◆ GT Designer3 (GOT2000) Version 1.103H or later
Even when the single touch operation is enabled in the object setting, you can disable and enable the operation with the device value (GS1794).
When b1 of the Gesture Common Control (GS1794) is on: Single touch operation is disabled.
When b1 of the Gesture Common Control (GS1794) is off: Single touch operation is enabled.
Note that when the single touch operation is disabled in the object setting, this signal does not work.
Even when the single touch operation is enabled in the object setting, you can disable and enable the operation with the device value (GS1794).
When b1 of the Gesture Common Control (GS1794) is on: Single touch operation is disabled.
When b1 of the Gesture Common Control (GS1794) is off: Single touch operation is enabled.
Note that when the single touch operation is disabled in the object setting, this signal does not work.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (standard function)
- Series
- GOT2000 Series
May I have your opinion?
Related FAQ
- Assigning a USB memory drive for the GOT2000 series
- Using with the GOT1000 series in a bus topology
- Use of commercially available USB memories for the GOT2000 series
- Compatibility of a commercially available wireless LAN access point
- Effect of attaching the protective cover for oil to the rugged model