Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23465
  • Release Date : 2018/09/14 15:06
  • Print

Operating the screen with the gesture function while using the SoftGOT-GOT link function

Answer

You cannot operate the screen of the GOT with the gesture function while using the SoftGOT-GOT link function, since GT SoftGOT2000 does not support the gesture function.

If GT SoftGOT2000 obtains the authorization while the GOT is in the screen gesture mode or displays the screen enlarged with a pinch-out operation, the GOT holds the screen gesture mode or display status, and GT SoftGOT2000 displays the normal-sized screen (100%) independently of the display status of the GOT.
After the authorization is transferred to the GOT, switching to the screen gesture mode is enabled on the GOT.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), SoftGOT
Series
GOT2000 Series, SoftGOT

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries