Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23473
  • Release Date : 2018/09/14 15:06
  • Print

Pinch-in operation of the screen gesture function

How much can I reduce the base screen with the pinch-out operation?
Category : 

Answer

You can reduce the base screen size enlarged with the pinch-out operation down to the normal size (100%) with the pinch-in operation. (You cannot reduce the screen size smaller than the normal size.)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?