Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23479
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/16 16:19
  • Print

Screen switching in screen gesture mode

Answer

When screen switching occurs in screen gesture mode, the following operations are performed.

• While the screen is touched
Removing your finger from the screen will switch the screen and disable screen gesture mode. 
• When the screen is not touched
The screen switches immediately and screen gesture mode is disabled.

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series, GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries