FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Canceling the screen gesture mode
FAQ
Canceling the screen gesture mode
How can I cancel the screen gesture mode?
Answer
You can cancel the screen gesture mode by the following methods.
・ Touch the screen gesture mode selector switch (key code: FF90).
・ Touch the full scale display (100%) switch (key code: FF91).
・ Switch to the utility screen.
・ Switch to the base screen.
・ Authorize VCN client when the GOT remote access function (VNC server function) is used.
・ Disable the authorization of the GOT network interaction function.
* Place the screen gesture mode selector switch outside the screen gesture active area.
* The full scale display (100%) switch is supported by GT Designer3 (GOT2000) Version 1.105K or later.
* The GOT network interaction function is supported by GT Designer3 (GOT2000) Version 1.144A or later.
・ Touch the screen gesture mode selector switch (key code: FF90).
・ Touch the full scale display (100%) switch (key code: FF91).
・ Switch to the utility screen.
・ Switch to the base screen.
・ Authorize VCN client when the GOT remote access function (VNC server function) is used.
・ Disable the authorization of the GOT network interaction function.
* Place the screen gesture mode selector switch outside the screen gesture active area.
* The full scale display (100%) switch is supported by GT Designer3 (GOT2000) Version 1.105K or later.
* The GOT network interaction function is supported by GT Designer3 (GOT2000) Version 1.144A or later.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series