FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Range of the screen display enlarged with the screen gesture function
FAQ
Range of the screen display enlarged with the screen gesture function
How can I determine which part of the normal screen is currently displayed in the screen enlarged with the screen gesture function?
Answer
◆ GT Designer3 (GOT2000) Version 1.105K or later
When the screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame consists of a bright red line only when the display contents inside the screen gesture active area are not enlarged, and a bright red line and dark red line when the display contents are enlarged. The length and position of the bright red line of the frame indicate where the enlarged display area corresponds the range in the full scale (100%) screen.
When the screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame consists of a bright red line only when the display contents inside the screen gesture active area are not enlarged, and a bright red line and dark red line when the display contents are enlarged. The length and position of the bright red line of the frame indicate where the enlarged display area corresponds the range in the full scale (100%) screen.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series