Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23483
  • Release Date : 2018/09/14 15:06
  • Update : 2018/10/04 13:26
  • Print

Checking the screen gesture mode

Can I check that the screen gesture mode is enabled on the screen?
Category : 

Answer

When the screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame consists of a bright red line only when the display contents inside the screen gesture active area are not enlarged, and a bright red line and dark red line when the display contents are enlarged. You can check that the screen gesture mode is enabled when this frame is displayed.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?