FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27 > Checking the screen gesture mode
FAQ
Checking the screen gesture mode
Can I check that the screen gesture mode is enabled on the screen?
Answer
When the screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame consists of a bright red line only when the display contents inside the screen gesture active area are not enlarged, and a bright red line and dark red line when the display contents are enlarged. You can check that the screen gesture mode is enabled when this frame is displayed.
This frame consists of a bright red line only when the display contents inside the screen gesture active area are not enlarged, and a bright red line and dark red line when the display contents are enlarged. You can check that the screen gesture mode is enabled when this frame is displayed.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series