Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23484
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 18:06
  • Print

Operating the object gesture function

What operations are available for the object gesture function of the GOT2000 series?
Category : 

Answer

The object gesture function of the GOT2000 series allows the time axis of a graph or document size to be enlarged or reduced with a pinch-in or pinch-out, and a graph or document pages to be scrolled with a swipe or slide.

The object gesture function can be used for the following objects.
・ Historical data list display
・ Alarm display (user)
・ Alarm display (system)
・ Simple alarm display
・ Historical trend graph
・ Document display
・ Video/RGB display object (* Not supported by GT2705-V)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries