Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23488
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 18:00
  • Print

Using with the GOT1000 series on the network

Answer

The GOT1000 series and GOT2000 series can be used together on the network if the network type is one of the following.
・ MELSECNET/H
・ CC-Link IE Controller Network
・ CC-Link IE Field Network
・ CC-Link (Intelligent device station/via G4)
・ Ethernet
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?