Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23491
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 17:36
  • Print

Use of a commercially available USB cable for the GOT2000 series

Answer

While you can use commercially available USB cables for the GOT2000 series, we have guaranteed the operation only when one of the following cables is used.
・ GT09-C30USB-5P
・ GT09-C20USB-5P (discontinued)
・ MR-J3USBCBL3M
 
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Cable
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?