Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23492
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 15:13
  • Print

Assigning a USB memory drive for the GOT2000 series

When I install a USB memory in a GOT2000 series model, which drive is assigned?
Category : 

Answer

The GOT2000 series can assign USB drives as follows.


For the details of the drive configuration, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"1.2.7 Drive configuration of the target GOT for data transfer"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (standard function)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?