Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23496
  • Release Date : 2018/09/14 15:06
  • Print

Using with the GOT1000 series in a GOT multi-drop topology

Can the GOT1000 series and GOT2000 series be used together in the GOT multi-drop topology?
Category : 

Answer

The GOT1000 series and GOT2000 series can be used together in the GOT multi-drop topology.

Use GT Designer3 (GOT1000) Version 1.12N or later to write the basic operating system and communication driver to the serial multi-drop connection unit (GT01-RS4-M).
The basic operating system and communication driver cannot be written with GT Designer3 (GOT2000).
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication), GOT function (multi-drop)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?