FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Checking the simultaneous 2-point press switches placed on the screen design software
FAQ
Checking the simultaneous 2-point press switches placed on the screen design software
Can I check the two switches placed at a location where the simultaneous 2-point press is invalid on the screen design software?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > Engineering Software > HMI/GOT Screen Design Software
Answer
You cannot check the two switches placed at a location where the simultaneous 2-point press is invalid on the screen design software. When creating a screen for the simultaneous 2-point press, display the simultaneous 2-point press invalid area on the drawing screen, and place the switches at a location where the simultaneous 2-point press is valid.
Display the simultaneous 2-point press invalid area as follows.
◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Right-click on the screen editor, and select [Two-point Press Inactive Area] - [Front] or [Back].
2. Select [View] - [Two-point Press Inactive Area] - [Front] or [Back] from the toolbar.
For restrictions on placement of simultaneous 2-point press switches, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"8.2.3 Precautions for a touch switch"
Display the simultaneous 2-point press invalid area as follows.
◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Right-click on the screen editor, and select [Two-point Press Inactive Area] - [Front] or [Back].
2. Select [View] - [Two-point Press Inactive Area] - [Front] or [Back] from the toolbar.
For restrictions on placement of simultaneous 2-point press switches, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"8.2.3 Precautions for a touch switch"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GT Designer3
- Series
- GOT2000 Series, Engineering Software
May I have your opinion?
Related FAQ
- Operating the screen with the gesture function while using the SoftGOT-GOT link function
- Location of the terminating resistor setting switch for the RS-422/485 communication port
- Using the rugged model in rain
- Upgrading the screen design software for the GOT2000 series
- Operating the objects with the gesture function using the SoftGOT-GOT link function