Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23513
  • Release Date : 2018/09/14 15:06
  • Print

Transferring the resource data from the GOT to a personal computer

Can I transfer the resource data, such as a logging file, from the GOT to a personal computer without using the screen design software?
Category : 

Answer

You can transfer the resource data of the GOT2000 series to a personal computer without using the screen design software in any of the following methods.

1. Use Data Transfer Tool (*1) to transfer the files.
2. Use the file transfer function (FTP transfer) to transfer the files.
(Available only for models with an Ethernet interface)
3. Use the file transfer function (GOT internal transfer) to transfer the files to an SD memory card or USB memory, and read the files from the personal computer.
4. Use the utility function to transfer the files to an SD memory card or USB memory, and read the files from the personal computer.

(*1) The Data Transfer Tool is supplied with GT Works3.
You can also download the tool from the Mitsubishi Electric FA Global Website.

For the details, refer to the following.
1. Help For Data Transfer Tool (BCN-P5670-AD)
 (got-data-trans-o.pdf in the installation destination folder)
 "4.2 Data Transfer Tool for GOT2000 Series"
 "5.1 Data Transfer with Command Line"
2. GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
 "10.15 Transferring a File between the GOT (FTP Server) and the Peripheral Device (FTP Client) (FTP Server Function)"
 "10.16 Transferring a File between the GOT (FTP Client) and Peripheral Device (FTP Server) (File Transfer Function (FTP Transfer))"
3. GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
 "10.17 Transferring a File between the GOT Drives (File Transfer Function (GOT Internal Transfer))"
4. GOT2000 Series User's Manual (Utility) (SH-081195)
 "6 DATA CONTROL"
 "15 CONTROL OF VARIOUS DATA (DATA CONTROL)"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (resource data transfer)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?