Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23520
  • Release Date : 2018/09/14 15:07
  • Print

Using the rugged model under the environment of strong external lights such as the afternoon sun

Can the rugged model be used under the environment of strong external lights such as the afternoon sun?
Category : 

Answer

The rugged model can be used under the environment of strong external lights such as the afternoon sun. Make sure that the operating ambient temperature does not exceed the specifications in the afternoon sun.
Since a high-intensity liquid crystal display panel is installed, the screen is displayable on the rugged model even in the bright places such as in the afternoon sun.
The brightness is adjustable in 32 levels.
Exposure to UV for a long time may turn the GOT front face in yellow.
Use the UV protective sheet (option) if the rugged model may be exposed to UV for a long period.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?