FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Using the rugged model in a walk-in freezer
FAQ
Using the rugged model in a walk-in freezer
Can the rugged model be used in a walk-in freezer?
Answer
The rugged model can be used in walk-in freezers that satisfy the following conditions.
・ Operating ambient temperature: -20°C to 65°C
・ Operating ambient humidity: 10% RH to 90% RH, non-condensing
The rugged model can be used in a wider operating ambient temperature range than any other models (operating ambient temperature: 0°C to 55°C).
・ Operating ambient temperature: -20°C to 65°C
・ Operating ambient humidity: 10% RH to 90% RH, non-condensing
The rugged model can be used in a wider operating ambient temperature range than any other models (operating ambient temperature: 0°C to 55°C).
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series