Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23531
  • Release Date : 2018/09/14 15:07
  • Update : 2018/09/25 17:18
  • Print

Setting a password to the rugged model

Answer

A password can be set to the rugged model.
A password can be set to the GOT individually for each case when the security is required.

・ Setting a password to change the contents of the screen display for each user
   → Level authentication or operator authentication
・ Setting a password to restrict invalid data reading and writing
   → Data transfer security
・ Setting a password to restrict the utility startup and password setting screen display
   → Functional operation security

For the details, refer to the following.
GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG-W)
"5.2.8 Configuring the security settings for displaying screen data on the GOT ([Screen Security] (Level authentication))"
"5.2.7 Configuring the security settings for displaying screen data on the GOT ([Screen Security] (Operator authentication))"
"5.2.10 Configuring the security setting for transferring data ([Data Transfer Security])"
"5.2.9 Configuring the security settings for operating the utility and the monitor functions ([Functional Operation Security])"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model, GOT function (screen security), GOT function (functional operation security), GOT function (operator authentication)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?