Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23538
  • Release Date : 2018/09/14 15:07
  • Update : 2018/09/25 17:16
  • Print

Using a USB interface on the control panel side of the rugged model

Can I use a USB interface on the control panel side of the rugged model?
Category : 

Answer

You can use a USB interface on the control panel of the rugged model by using the panel-mounted USB port extension.
・ GT14-C10EXUSB-4S: Cable for routing the USB interface (host) on the GOT rear face to the control panel side (front side)
・ GT10-C10EXUSB-5S: Cable for routing the USB interface (device) on the GOT rear face to the control panel side (front side)
* The panel-mounted USB port extension does not conform to IP66F.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model, cable
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?