Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23594
  • Release Date : 2018/09/14 15:09
  • Print

Input/output signal

Currently, NPN photo sensor is being used for upper/lower stroke limit and proximity dog signals, but no signal is received.
What should I do?
Category : 

Answer

Check if 24 VDC power is supplied to "1A7" (pin No.) of the external input signal connector.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC-Q
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?