Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23613
  • Release Date : 2018/09/14 15:09
  • Print

Error 108

Answer

Error 108 (Start not possible) occurs when a start is requested while a stop signal is ON.
Check the "[Md.26] Axis operation status".If "20: Servo amplifier has not been connected/servo amplifier power OFF" is set, turn ON the control circuit of the servo amplifier.
Be sure not to request a start when the axis operation state is other
than "0: standby", "1: stopped", and "-2: step standby".
Product Name
Simple Motion module/
Positioning module
Series
MELSEC-Q
MELSEC-L
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?