Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23617
  • Release Date : 2018/09/14 15:09
  • Print

HPR request flag

Answer

It depends on the setting of servo parameter "[PA03] Absolute position detection system" whether the HPR request flag ("[Md.31] Status": b3) turns ON or not.
The flag turns ON in the following cases:
(1) "1: Enabled (absolute position detection system)"
    • When the machine HPR has not been executed at the absolute position system
    • When a machine HPR operation starts
    • When the absolute system has not been set
    • When "[PA14] Rotation direction selection/travel direction selection" is changed
(2) "0: Disabled (incremental system)"
    • System's power supply on or reset
    • Servo amplifier power supply on
    • Machine HPR start
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?