FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Error of the communication option
FAQ
Error of the communication option
What is the difference between E.OP1 and E.1?
- Category :
Answer
E.OP1 indicates the communication line error. E.1 indicates a hardware fault of the communication option. (It is judged as the hardware fault when the communication option cannot communicate with the inverter.) For E.1, the inverter trips regardless of the Pr.502 setting.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option