Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20811
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800/FR-F800

The Instruction Manual of the E700 describes that the one rotation of the setting dial is 24 clicks. Is one rotation of the setting dial is also 24 clicks for the 800 series?
Category : 

Answer

It is 30 clicks the FR-A800/FR-F800.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?