Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20816
  • Release Date : 2018/08/22 16:24
  • Print

TH3 terminal of the MT-BR5

There are TH1, TH2, TH3, and E terminals on the control circuit terminal block. What is the TH3 used for?
Category : 

Answer

The resistor unit MT-BR5 manufactured in February 2016 or later has output terminal TH3 (NC contact) as a fault output terminal.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?