FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Combination of the FR-F800 and MM-EFS
FAQ
Combination of the FR-F800 and MM-EFS
Can the MM-EFS of one-rank lower capacity be used with the FR-F800?
- Category :
Answer
Yes, it can. Set "12" or "112" to the MM-EFS capacity used for Pr.80 (Motor capacity) and Pr.998 (PM parameter initialization).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-F800