FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > Engineering Software > Seamless communication of FR Configurator SW3
FAQ
Seamless communication of FR Configurator SW3
The master and remote I/O station of the programmable controller is connected via the MELSECNET and the inverter is connected to the CC-Link unit of remote I/O. With this configuration, is the CC-Link Seamless communication available?
- Category :
Answer
The communication via the MELSECNET is not available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR Configurator SW3