FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Safety stop function of the FR-D700/FR-E700
FAQ
Safety stop function of the FR-D700/FR-E700
Can the category 3 be satisfied even when the magnetic contactor, which is described as the safety stop function connection example in the Instruction Manual, is not installed on the input side of the inverter?
- Category :
Answer
It is recommended to install the magnetic contactor on the input side of the inverter for safety. The category 3 can be satisfied without installing it.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-D700, FR-E700