FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800-E
FAQ
FR-A800-E
For the CC-Link IE Field BASIC specification, what is (open specification) written with the number of connectable inverters in the Instruction Manual?
- Category :
Answer
It indicate that the actual number of connectable units differs depending on the master side specification although the maximum number of connectable units on the inverter side is 64. (When the maximum number of connectable units on the master side is less than 64, the maximum number of connectable units on the inverter side is the same as that of the master side.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-E