Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20846
  • Release Date : 2018/08/22 16:24
  • Print

Selection method of the FR-ABR

The selection of the FR-ABR is changed from "Select by the motor capacity" to "Select by the inverter capacity". Why is it?
Category : 

Answer

The multiple rating is adopted from the FR-A800 series and the motor and the inverter are no longer one-to-one. Thus, considering the combination that the motor capacity exceeds the inverter capacity, the selection method is changed to adjust along with the capacity of the inverter.
Product Name
Inverter, magnet motor drive
Product Category
Option
Series
Option
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?