FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Selection method of the FR-ABR
FAQ
Selection method of the FR-ABR
The selection of the FR-ABR is changed from "Select by the motor capacity" to "Select by the inverter capacity". Why is it?
- Category :
Answer
The multiple rating is adopted from the FR-A800 series and the motor and the inverter are no longer one-to-one. Thus, considering the combination that the motor capacity exceeds the inverter capacity, the selection method is changed to adjust along with the capacity of the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Option
- Series
- Option