Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20848
  • Release Date : 2018/08/22 16:24
  • Print

High speed sampling of FR Configurator2

Is the high speed sampling of the graph available when the FR-A800-E is connected via the Ethernet?
Category : 

Answer

High speed sampling is not available. Only the normal sampling is available.
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR Configurator2
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?