FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Emergency stop of the FR-A800
FAQ
Emergency stop of the FR-A800
When the emergency stop (X92) signal turns ON, the FR-A800 is decelerated to stop by the setting of Pr.1103 Deceleration time at emergency stop and Pr.815 Torque limit level 2. Pr.815 is disabled when the V/F control or Advanced magnetic flux vector control is performed. What will happen in this case?
- Category :
Answer
For the V/F control and Advanced magnetic flux vector control, the FR-A800 stops only by Pr.1103 Deceleration time at emergency stop. Pr.815 is not affected.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800