Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20863
  • Release Date : 2018/08/22 16:24
  • Print

FR-F800

Does the BACnet MS/TP protocol communication of the FR-F800 conform to the ISO standards?
Category : 

Answer

Yes, it does, however, it does not acquire the certification of the BACnet association standard.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?