FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > FR-A800
FAQ
FR-A800
Do the metallic sound of the motor and leakage current at the offline auto tuning change according to the value of Pr.72 (PWM frequency selection)?
- Category :
Answer
No, they do not. Pr.72 is invalid at the offline auto tuning. It is also invalid when the motor rotates with Pr.96 = 101.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800