FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > FR-A800-E
FAQ
FR-A800-E
What type of connection path is used for FR Configurator2?
- Category :
Answer
The direct connection with the inverter like the standard model, and the connection via the GOT and relay station (programmable controller) are available. Only Q and L series are supported by the connection via the programmable controller. (The R series is also supported from Ver.1.10L)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-E, FR-F800-E