FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > FR-A800-E
FAQ
FR-A800-E
Is the RS-485 communication possible?
- Category :
Answer
It is not possible because the RS-485 terminal block is not installed. Use the FR-A800 (RS-485 communication type) when performing the RS-485 communication.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-E, FR-F800-E