Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20882
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-E

What is required for building the Ethernet communication network?
Category : 

Answer

The RJ-45 compatible connector (LAN cable), switching hub, and others are required The auto detection of the connection devices, externally monitoring the inverter status, and parameter settings become possible by using FR Configurator2.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?