FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A800-E
FAQ
FR-A800-E
Can the same options as the FR-A800 (RS-485 communication type) be used for the FR-A800-E?
- Category :
Answer
There are some restrictions compared to the FR-A800 (RS-485 communication type). For example, the FR-A8TR is unavailable, and only two option connectors are unoccupied.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800-E, FR-F800-E