Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20891
  • Release Date : 2018/08/22 16:24
  • Print

FR-A800-R2R

The normal speed control is performed when X114 is turned OFF. Can I use the second terminal as a frequency setting value when Pr.361 is set? I want to use the second terminal for the line speed command and frequency setting in the normal mode.
Category : 

Answer

If Pr.361 = 0, the second terminal can be used as the line speed command when X114 is ON, and as the frequency setting value when X114 is OFF. If Pr.361 = 3, the second terminal does not function as the frequency setting when X114 is OFF.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800-R2R
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?