FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F800 > Reduced impact restart
FAQ
Reduced impact restart
It is described that the reduced impact restart of Pr.162 = 3 or 13, which is added from the 800 series, enables the further smooth start reducing the impact compared to the one with 0 or 10. What control is performed exactly?
- Category :
Answer
Until now the DC has been applied to perform the frequency search. When Pr.162 = 3 or 13, the impact is reduced by detecting the phase and performing the search in the AC application method.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800