FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Engineering Software > FR Configurator2
FAQ
FR Configurator2
What is the difference between the high speed sampling "Output current" and "Output current (three-phase full-wave)" displayed on the graph?
- Category :
Answer
Output current: Because the filter, effective value of the output current displayed on the operation panel, is included, the momentary fluctuation is difficult to be checked.
Output current (for all three phases): The momentary fluctuation can be checked with the maximum output current value at the U phase, V phase, and W phase. Note that it must be divided by 2 for the effective value conversion.
Effective value of the output current = Maximum value of the output current/2
Output current (for all three phases): The momentary fluctuation can be checked with the maximum output current value at the U phase, V phase, and W phase. Note that it must be divided by 2 for the effective value conversion.
Effective value of the output current = Maximum value of the output current/2
- Product Name
- Inverter, magnet motor drive
- Product Category
- Engineering software
- Series
- FR Configurator2