Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20919
  • Release Date : 2018/08/22 16:25
  • Print

FR Configurator2

What is the difference between the high speed sampling "Output current" and "Output current (three-phase full-wave)" displayed on the graph?
Category : 

Answer

Output current: Because the filter, effective value of the output current displayed on the operation panel, is included, the momentary fluctuation is difficult to be checked.
Output current (for all three phases): The momentary fluctuation can be checked with the maximum output current value at the U phase, V phase, and W phase. Note that it must be divided by 2 for the effective value conversion.
Effective value of the output current = Maximum value of the output current/2
Product Name
Inverter, magnet motor drive
Product Category
Engineering software
Series
FR Configurator2
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?