FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800-GF
FAQ
FR-A800-GF
Can the same options as the FR-A800 be used for the FR-A800-GF?
- Category :
Answer
Yes, the options are the same as the FR-A800 standard model. Note that two options can be added at maximum. (One option is already used as standard.) Other communication options are unavailable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800