FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Waiting time at the instantaneous power failure
FAQ
Waiting time at the instantaneous power failure
Fro instantaneous power failure, when the waiting time is set with Pr.57, which is the counting start, at power failure or at power restoration?
- Category :
Answer
The count is started from the power failure. The count is started after the power restoration or reset release when the power failure period is too long, or when the control circuit cannot be held.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800, FR-D700, FR-E700, FR-E700EX