FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > Input phase loss protection
FAQ
Input phase loss protection
Why is the initial value of Pr.872 (Input phase loss protection) "1" (Valid) for the A701 and "0" (Invalid) for the A700?
- Category :
Answer
The initial value of Pr.872 is set to "1" (Valid) because the A701 have regeneration unit built-in and an overvoltage may occur when the regenerative operation is performed at an input phase loss.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700