Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20957
  • Release Date : 2018/08/22 16:25
  • Print

Emergency stop function

It is described that when the emergency stop function (X92) is used, the deceleration stop is performed according to the setting in Pr.815 Torque limit level 2. What happens under V/F control?
Category : 

Answer

The deceleration stop is also performed according to the setting in Pr.815 under V/F control.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?