Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 20958
  • Release Date : 2018/08/22 16:25
  • Print

Storage area

It is described that the parameters for the PLC function and sequence programs are written to the flash memory and the number of writing times is limited (about 1,000,000 times). Is this storage area different from that of the EEPROM for the parameters of the inverter?
Category : 

Answer

The storage areas for the sequence programs and for the parameters of the inverter are different.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?