FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Parameter copy to the USB memory
FAQ
Parameter copy to the USB memory
Can I read parameters to the USB memory during operation?
- Category :
Answer
Yes. Parameters can be read except during an inverter reset or when the password function is set.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800